Basics of Phase Change Memory

Phase Change Memory (PCM) animation
Catalog
Ⅰ Introduction
Phase change random access memory, P-RAM, is a type of non-volatile memory or computer storage that is faster than the Flash memory system that is far more widely used. A variety of terms, like P-RAM or PRAM, PC-RAM, phase change RAM, and probably more, may be used to refer to phase change memory. Phase shift memory is based on a technique originally developed by Hewlett Packard, known as the memresitor.
A number of other suppliers have also taken up phase shift memory and are expected to see growing use. Phase shift memory is seen as a big development and one that is expected to become one of the future standard semiconductor memory formats.
The phase change memory, PCM, or random access memory of phase change, P-RAM, uses the special property of a material called chalcogenide glass.

Phase Change Memory
The P-RAM uses the fact that the chalcogenide glass shifts through the passing of current that generates heat when it travels through a cell into two states, polycrystalline and amorphous. As the material transitions between the two states or stages, this gives rise to the term phase transition.
The substance displays a high degree of resistance and even poor reflectivity in the amorphous state.

Architecture of PCM
The substance has a normal crystalline form in the polycrystalline state, and this expresses itself in a change in properties. It has a low resistance in this state so electrons can pass freely through the crystalline structure, and it also shows a high reflectivity.
It is the resistance level that is of concern for phase shift storage / phase change RAM. The circuitry around the cell then senses the resistance shift when the two states have a different resistance and then detects if there is a "1" or "0" stored in that position.
As a result of injection current for a timed duration, the phase transition between the two states of the chalcogenide is brought on by localized heating. The amplitude of the injected current and the time of the process modulate the final step of the substance.
The heating is given by a resistive element - it reaches from the bottom electrode to the chalcogenide base. Heat that is then transmitted to the chalcogenide layer is given by the current passing through the resistive heater portion. In addition, two additional states have recently developed the technology, essentially doubling the storage of a given-sized unit.
The promise of PCM has been seen in a wide variety of works over the past 10 years as a pure memory technology, and the only remaining problems are arguably linked to cost, product-level development and high-level incorporation into a computer device. The successful introduction of Intel Optane in 2018, a PCM-based non-volatile memory that can be used to boost the current memory storage infrastructure, shows the possibility of using PCM in a traditional operating system as a digital memory. Because of this, a thorough understanding of PCM's fundamental physical processes and state dynamics is necessary for working out how to further refine the technology.
Ⅱ Advantages & disadvantages
1.Advantages of phase change memory
Non-volatile: Phase change RAM is a non-volatile type of memory, i.e. the retention of its data does not require power. This helps it to specifically compete with flash memory.
Bit alterable: P-RAM / PCM is what is considered bit-alterable, equivalent to RAM or EEPROM. This means that without the need for a deleting process, data can be written directly to it. This gives it a major advantage over flash that needs a period of deletion before it can be written to new files.
Fast read performance: Rapid random access times are given by Phase change RAM, P-RAM / PCM. This has the bonus that it allows code to be run directly from the memory, without the need to copy the data to RAM. The P-RAM read latency is equivalent to one bit per NOR flash cell, while the read bandwidth is close to that of DRAM.
Fast read performance: Phase change RAM, P-RAM / PCM features fast random access times. This has the bonus that it allows code to be run directly from the memory, without the need to copy the data to RAM. The P-RAM read latency is equivalent to one bit per NOR flash cell, while the read bandwidth is close to that of DRAM.
Scalability: Another aspect where it may have benefits is the scalability of P-RAM for the future, but this is yet to be understood. The logic is that both NOR and NAND flash variants depend on hard-to-shrink floating gate memory structures. If the memory cell size is decreased, it is observed that the amount of electrons deposited on the floating gate is reduced and this makes it more difficult to identify these smaller charges accurately. P-RAM does not store a charge, but depends on a shift in resistance instead. As a consequence, it is not vulnerable to the same issues of scaling.
Write/erase performance: phase change memory's erase performance is very strong with higher speeds and lower latency than NAND flash. Because no deletion phase is needed, this offers a major overall improvement over flash.
2.Disadvantages of phase change memory
Economic viability: Despite the numerous promises regarding the benefits of P-RAM, few enterprises have been able to produce chips that have been commercialized successfully.
Multiple bit storage per Flash cell: Flash's ability to store and detect multiple bits per cell also gives Flash an advantage over P-RAM in memory space. Although P-RAM / PCM has benefits for the future in potential scalability.
Both the positives and drawbacks need to be weighed when looking at using phase change memory.
A number of manufacturers have implemented phase change memory, but it is still not commonly used as many developers might be skeptical of a modern invention like this. Nevertheless, PCM has many distinct benefits to deliver on a variety of instances in phase change memory.
Ⅲ Different Companies’ Phase Change Memory
As described above, phase change memory is a product that is seeing substantial investment from major suppliers. Multiple manufacturers have been openly discussing their PCM activities and technologies with differing degrees of success at this stage.
IBM
PCM storage innovations working on its OpenPower server architecture have been shown by IBM.
A three bit per cell PCM chip is among IBM's research developments, which could provide more stability and storage than previous research which demonstrated 1 bit per cell options.
Intel
Since at least 2006, Intel has been working on PCM, when it unveiled the platform at its developer conference.
Any components of PCM may be part of the 3D XPoint technologies of the business, but a dedicated PCM solution is not currently directly advertised by Intel.
Micron
Thanks in part to its 2010 purchase of PCM leader Numonyx, Micron has been among the leading suppliers developing PCM technology.
Micron revealed that it was leaving the PCM market in 2014 following several fits and starts.
Samsung
For over a decade, Samsung has been focusing on diverse versions of PCM technology.
The key use case that the business is currently working on is for embedded use inside mobile phones, but there is still the possibility for possible commercial storage systems.
STMicroelectronics
One of the core patents that allows PCM storage is held by STMicrolectonics.
For automotive use cases, the company has been developing embedded PCM (ePCM) technology.
Digital Western
The HGST (Hitachi Global Storage Technologies) business unit of Western Digital has been developing a technology called DC Express to help fully enable PCM storage for a future motherboard generation.
1.What is a phase change memory device?
Phase-change memory (PCM) is a key enabling technology for non-volatile electrical data storage at the nanometer scale. A PCM device consists of a small active volume of phase-change material sandwiched between two electrodes. The stored data can be retrieved by measuring the electrical resistance of the PCM device.
2.What are the challenges in the phase change memory?
Probably the biggest challenge for phase-change memory is its long-term resistance and threshold voltage drift. The resistance of the amorphous state slowly increases according to a power law (~t0.1).
3.What are PCMs used for?
PCMs are used in many different commercial applications where energy storage and/or stable temperatures are required, including, among others, heating pads, cooling for telephone switching boxes, and clothing. By far the biggest potential market is for building heating and cooling.
High-Capacity HDDs in the AI Era: Sourcing Massive Storage for Cold DataUTMEL04 July 2026693As generative AI and LLMs drive an explosion of unstructured data, high-capacity enterprise HDDs remain the most cost-effective solution for cold storage. Despite rising prices and supply chain bottlenecks, mechanical drives offer a massive cost-per-gigabyte advantage over SSDs. Technologies like HAMR and SMR enable capacities beyond 24TB, though deploying these drives requires robust RAID 6 strategies and secured IC supply chains to mitigate rebuilding and procurement risks.
Read More
LPDDR5 Memory 2026: Lead Times, HBM Impact, and Procurement StrategiesUTMEL17 July 20264489Global semiconductor fabrication facility managing advanced memory production. In Q2 2026, contract prices for 12GB LPDDR5X modules surged 89% quarter-over-quarter, jumping from $77.10 to $145.90, while lead times for advanced memory components stretched to 40–58 weeks. A vehicle platform designed in 2023 with specific memory requirements must ship in 2026, regardless of spot market conditions.
Read More
2026 DRAM and the 3-to-1 HBM Rule: Market Supply Analysis and B2B Procurement GuideUTMEL23 July 20265789This technical report explains how the physical "3-to-1 wafer penalty" of High Bandwidth Memory (HBM) production has cannibalized standard DRAM capacity, causing severe shortages of DDR4 and DDR5 in 2026. As major hardware OEMs pass these soaring component costs directly to enterprise buyers, procurement teams must abandon Just-in-Time models in favor of rolling safety stocks and strategic long-term distributor agreements to protect budgets.
Read More
Automotive vs. Industrial Memory: How to Verify Grade Codes Before Sourcing In this guideUTMEL06 August 2026479Memory ordering codes can look almost identical while representing different temperature limits, packages, revisions, qualification evidence, or lifecycle commitments. For automotive and long-life industrial designs, the safe purchasing unit is the complete manufacturer ordering code, not a base part number plus a familiar-looking suffix.
Read More
How to Use an External Hard Drive?UTMEL24 June 20219462The external hard drive is a compact and portable hard drive storage which can be plugged in or unplugged at any time. It mainly uses USB or IEEE1394 interfaces. It can transmit data with the system at a higher speed. The IEEE 1394 interface transfer rate is 50-100 MB/s.
Read More
Subscribe to Utmel !
36HNSP.25Remington Industries
25/38LITZ.125Remington Industries
260/38LITZ.125Remington Industries
34HNSP.125Remington Industries
17HNSP.125Remington Industries
21HNSRemington Industries
31HNSP.5Remington Industries
38HNS2.5Remington Industries
15HNSP.5Remington Industries
17HNSRemington Industries


Product
Brand
Articles
Tools